- Introduction
- Configuring Manager Application Access
- HTML User-friendly Interface
- Supported Manager Commands
- Common Parameters
- Deploy A New Application Archive (WAR) Remotely
- Deploy A New Application from a Local Path
- List Currently Deployed Applications
- Reload An Existing Application
- List OS and JVM Properties
- List Available Global JNDI Resources
- Session Statistics
- Expire Sessions
- Start an Existing Application
- Stop an Existing Application
- Undeploy an Existing Application
- Finding memory leaks
- Connector SSL/TLS cipher information
- Connector SSL/TLS certificate chain information
- Connector SSL/TLS trusted certificate information
- Reload TLS configuration
- Thread Dump
- VM Info
- Save Configuration
- Server Status
- Using the JMX Proxy Servlet
- Executing Manager Commands With Ant
Manager App HOW-TO
Table of Contents
Introduction
In many production environments, it is very useful to have the capability
to deploy a new web application, or undeploy an existing one, without having
to shut down and restart the entire container. In addition, you can request
an existing application to reload itself, even if you have not declared it
to be reloadable
in the Tomcat server
configuration file.
To support these capabilities, Tomcat includes a web application
(installed by default on context path /manager
) that supports
the following functions:
- Deploy a new web application from the uploaded contents of a WAR file.
- Deploy a new web application, on a specified context path, from the server file system.
- List the currently deployed web applications, as well as the sessions that are currently active for those web apps.
- Reload an existing web application, to reflect changes in the
contents of
/WEB-INF/classes
or/WEB-INF/lib
. - List the OS and JVM property values.
- List the available global JNDI resources, for use in deployment
tools that are preparing
<ResourceLink>
elements nested in a<Context>
deployment description. - Start a stopped application (thus making it available again).
- Stop an existing application (so that it becomes unavailable), but do not undeploy it.
- Undeploy a deployed web application and delete its document base directory (unless it was deployed from file system).
A default Tomcat installation includes the Manager. To add an instance of the
Manager web application Context
to a new host install the
manager.xml
context configuration file in the
$CATALINA_BASE/conf/[enginename]/[hostname]
folder. Here is an
example:
<Context privileged="true" antiResourceLocking="false"
docBase="${catalina.home}/webapps/manager">
<Valve className="org.apache.catalina.valves.RemoteAddrValve"
allow="127\.0\.0\.1" />
</Context>
If you have Tomcat configured to support multiple virtual hosts (websites) you would need to configure a Manager for each.
There are three ways to use the Manager web application.
- As an application with a user interface you use in your browser.
Here is an example URL where you can replace
localhost
with your website host name:http://localhost:8080/manager/html
. - A minimal version using HTTP requests only which is suitable for use by scripts setup by system administrators. Commands are given as part of the request URI, and responses are in the form of simple text that can be easily parsed and processed. See Supported Manager Commands for more information.
- A convenient set of task definitions for the Ant (version 1.4 or later) build tool. See Executing Manager Commands With Ant for more information.
Configuring Manager Application Access
The description below uses the variable name $CATALINA_BASE to refer the base directory against which most relative paths are resolved. If you have not configured Tomcat for multiple instances by setting a CATALINA_BASE directory, then $CATALINA_BASE will be set to the value of $CATALINA_HOME, the directory into which you have installed Tomcat.
It would be quite unsafe to ship Tomcat with default settings that allowed
anyone on the Internet to execute the Manager application on your server.
Therefore, the Manager application is shipped with the requirement that anyone
who attempts to use it must authenticate themselves, using a username and
password that have one of manager-xxx roles associated with
them (the role name depends on what functionality is required).
Further, there is no username in the default users file
($CATALINA_BASE/conf/tomcat-users.xml
) that is assigned to those
roles. Therefore, access to the Manager application is completely disabled
by default.
You can find the role names in the web.xml
file of the Manager
web application. The available roles are:
- manager-gui — Access to the HTML interface.
- manager-status — Access to the "Server Status" page only.
- manager-script — Access to the tools-friendly plain text interface that is described in this document, and to the "Server Status" page.
- manager-jmx — Access to JMX proxy interface and to the "Server Status" page.
The HTML interface is protected against CSRF (Cross-Site Request Forgery) attacks, but the text and JMX interfaces cannot be protected. It means that users who are allowed access to the text and JMX interfaces have to be cautious when accessing the Manager application with a web browser. To maintain the CSRF protection:
- If you use web browser to access the Manager application using a user that has either manager-script or manager-jmx roles (for example for testing the plain text or JMX interfaces), you MUST close all windows of the browser afterwards to terminate the session. If you do not close the browser and visit other sites, you may become victim of a CSRF attack.
- It is recommended to never grant the manager-script or manager-jmx roles to users that have the manager-gui role.
Note that JMX proxy interface is effectively low-level root-like administrative interface of Tomcat. One can do a lot, if he knows what commands to call. You should be cautious when enabling the manager-jmx role.
To enable access to the Manager web application, you must either create a new username/password combination and associate one of the manager-xxx roles with it, or add a manager-xxx role to some existing username/password combination. As the majority of this document describes the using the text interface, this example will use the role name manager-script. Exactly how the usernames/passwords are configured depends on which Realm implementation you are using:
- UserDatabaseRealm plus MemoryUserDatabase, or MemoryRealm
— The UserDatabaseRealm and MemoryUserDatabase are
configured in the default
$CATALINA_BASE/conf/server.xml
. Both MemoryUserDatabase and MemoryRealm read an XML-format file by default stored at$CATALINA_BASE/conf/tomcat-users.xml
, which can be edited with any text editor. This file contains an XML<user>
for each individual user, which might look something like this:which defines the username and password used by this individual to log on, and the role names he or she is associated with. You can add the manager-script role to the comma-delimited<user username="craigmcc" password="secret" roles="standard,manager-script" />
roles
attribute for one or more existing users, and/or create new users with that assigned role. - DataSourceRealm or JDBCRealm — Your user and role information is stored in a database accessed via JDBC. Add the manager-script role to one or more existing users, and/or create one or more new users with this role assigned, following the standard procedures for your environment.
- JNDIRealm — Your user and role information is stored in a directory server accessed via LDAP. Add the manager-script role to one or more existing users, and/or create one or more new users with this role assigned, following the standard procedures for your environment.
The first time you attempt to issue one of the Manager commands described in the next section, you will be challenged to log on using BASIC authentication. The username and password you enter do not matter, as long as they identify a valid user in the users database who possesses the role manager-script.
In addition to the password restrictions, access to the Manager web
application can be restricted by the remote IP address or host
by adding a RemoteAddrValve
or RemoteHostValve
.
See valves documentation
for details. Here is
an example of restricting access to the localhost by IP address:
<Context privileged="true">
<Valve className="org.apache.catalina.valves.RemoteAddrValve"
allow="127\.0\.0\.1"/>
</Context>
HTML User-friendly Interface
The user-friendly HTML interface of Manager web application is located at
http://{host}:{port}/manager/html
As has already been mentioned above, you need manager-gui role to be allowed to access it. There is a separate document that provides help on this interface. See:
The HTML interface is protected against CSRF (Cross-Site Request Forgery) attacks. Each access to the HTML pages generates a random token, which is stored in your session and is included in all links on the page. If your next action does not have correct value of the token, the action will be denied. If the token has expired you can start again from the main page or List Applications page of Manager.
Supported Manager Commands
All commands that the Manager application knows how to process are specified in a single request URI like this:
http://{host}:{port}/manager/text/{command}?{parameters}
where {host}
and {port}
represent the hostname
and port number on which Tomcat is running, {command}
represents the Manager command you wish to execute, and
{parameters}
represents the query parameters
that are specific to that command. In the illustrations below, customize
the host and port appropriately for your installation.
The commands are usually executed by HTTP GET requests. The
/deploy
command has a form that is executed by an HTTP PUT request.
Common Parameters
Most commands accept one or more of the following query parameters:
- path - The context path (including the leading slash)
of the web application you are dealing with. To select the ROOT web
application, specify "/".
NOTE: It is not possible to perform administrative commands on the Manager application itself.
NOTE: If the path parameter is not explicitly specified then the path and the version will be derived using the standard Context naming rules from the config parameter or, if the config parameter is not present, the war parameter. - version - The version of this web application as used by
the parallel deployment feature. If you
use parallel deployment wherever a path is required you must specify a
version in addition to the path and it is the combination of path and
version that must be unique rather than just the path.
NOTE: If the path is not explicitly specified, the version parameter is ignored. - war - URL of a web application archive (WAR) file, or
pathname of a directory which contains the web application, or a
Context configuration ".xml" file. You can use URLs in any of the
following formats:
- file:/absolute/path/to/a/directory - The absolute path of a directory that contains the unpacked version of a web application. This directory will be attached to the context path you specify without any changes.
- file:/absolute/path/to/a/webapp.war - The absolute
path of a web application archive (WAR) file. This is valid
only for the
/deploy
command, and is the only acceptable format to that command. - file:/absolute/path/to/a/context.xml - The absolute path of a web application Context configuration ".xml" file which contains the Context configuration element.
- directory - The directory name for the web application context in the Host's application base directory.
- webapp.war - The name of a web application war file located in the Host's application base directory.
Each command will return a response in text/plain
format
(i.e. plain ASCII with no HTML markup), making it easy for both humans and
programs to read). The first line of the response will begin with either
OK
or FAIL
, indicating whether the requested
command was successful or not. In the case of failure, the rest of the first
line will contain a description of the problem that was encountered. Some
commands include additional lines of information as described below.
Internationalization Note - The Manager application looks up its message strings in resource bundles, so it is possible that the strings have been translated for your platform. The examples below show the English version of the messages.
Deploy A New Application Archive (WAR) Remotely
http://localhost:8080/manager/text/deploy?path=/foo
Upload the web application archive (WAR) file that is specified as the
request data in this HTTP PUT request, install it into the appBase
directory of our corresponding virtual host, and start, deriving the name for
the WAR file added to the appBase
from the specified path. The
application can later be undeployed (and the corresponding WAR file removed) by
use of the /undeploy
command.
This command is executed by an HTTP PUT request.
The .WAR file may include Tomcat specific deployment configuration, by
including a Context configuration XML file in
/META-INF/context.xml
.
URL parameters include:
update
: When set to true, any existing update will be undeployed first. The default value is set to false.tag
: Specifying a tag name, this allows associating the deployed webapp with a tag or label. If the web application is undeployed, it can be later redeployed when needed using only the tag.
NOTE - This command is the logical
opposite of the /undeploy
command.
If installation and startup is successful, you will receive a response like this:
OK - Deployed application at context path /foo
Otherwise, the response will start with FAIL
and include an
error message. Possible causes for problems include:
- Application already exists at path /foo
The context paths for all currently running web applications must be unique. Therefore, you must undeploy the existing web application using this context path, or choose a different context path for the new one. The
update
parameter may be specified as a parameter on the URL, with a value oftrue
to avoid this error. In that case, an undeploy will be performed on an existing application before performing the deployment. - Encountered exception
An exception was encountered trying to start the new web application. Check the Tomcat logs for the details, but likely explanations include problems parsing your
/WEB-INF/web.xml
file, or missing classes encountered when initializing application event listeners and filters.
Deploy A New Application from a Local Path
Deploy and start a new web application, attached to the specified context
path
(which must not be in use by any other web application).
This command is the logical opposite of the /undeploy
command.
This command is executed by an HTTP GET request. There are a number of different ways the deploy command can be used.
Deploy a previously deployed webapp
http://localhost:8080/manager/text/deploy?path=/footoo&tag=footag
This can be used to deploy a previously deployed web application, which
has been deployed using the tag
attribute. Note that the work
directory of the Manager webapp will contain the previously deployed WARs;
removing it would make the deployment fail.
Deploy a Directory or WAR by URL
Deploy a web application directory or ".war" file located on the Tomcat
server. If no path
is specified, the path and version are derived
from the directory name or the war file name. The war
parameter
specifies a URL (including the file:
scheme) for either
a directory or a web application archive (WAR) file. The supported syntax for
a URL referring to a WAR file is described on the Javadocs page for the
java.net.JarURLConnection
class. Use only URLs that refer to
the entire WAR file.
In this example the web application located in the directory
/path/to/foo
on the Tomcat server is deployed as the
web application context named /footoo
.
http://localhost:8080/manager/text/deploy?path=/footoo&war=file:/path/to/foo
In this example the ".war" file /path/to/bar.war
on the
Tomcat server is deployed as the web application context named
/bar
. Notice that there is no path
parameter
so the context path defaults to the name of the web application archive
file without the ".war" extension.
http://localhost:8080/manager/text/deploy?war=file:/path/to/bar.war
Deploy a Directory or War from the Host appBase
Deploy a web application directory or ".war" file located in your Host appBase directory. The path and optional version are derived from the directory or war file name.
In this example the web application located in a sub directory named
foo
in the Host appBase directory of the Tomcat server is
deployed as the web application context named /foo
. Notice
that the context path used is the name of the web application directory.
http://localhost:8080/manager/text/deploy?war=foo
In this example the ".war" file bar.war
located in your
Host appBase directory on the Tomcat server is deployed as the web
application context named /bar
.
http://localhost:8080/manager/text/deploy?war=bar.war
Deploy using a Context configuration ".xml" file
If the Host deployXML flag is set to true you can deploy a web
application using a Context configuration ".xml" file and an optional
".war" file or web application directory. The context path
is not used when deploying a web application using a context ".xml"
configuration file.
A Context configuration ".xml" file can contain valid XML for a
web application Context just as if it were configured in your
Tomcat server.xml
configuration file. Here is an
example:
<Context path="/foobar" docBase="/path/to/application/foobar">
</Context>
When the optional war
parameter is set to the URL
for a web application ".war" file or directory it overrides any
docBase configured in the context configuration ".xml" file.
Here is an example of deploying an application using a Context configuration ".xml" file.
http://localhost:8080/manager/text/deploy?config=file:/path/context.xml
Here is an example of deploying an application using a Context configuration ".xml" file and a web application ".war" file located on the server.
http://localhost:8080/manager/text/deploy
?config=file:/path/context.xml&war=file:/path/bar.war
Deployment Notes
If the Host is configured with unpackWARs=true and you deploy a war file, the war will be unpacked into a directory in your Host appBase directory.
If the application war or directory is installed in your Host appBase directory and either the Host is configured with autoDeploy=true or the Context path must match the directory name or war file name without the ".war" extension.
For security when untrusted users can manage web applications, the Host deployXML flag can be set to false. This prevents untrusted users from deploying web applications using a configuration XML file and also prevents them from deploying application directories or ".war" files located outside of their Host appBase.
Deploy Response
If installation and startup is successful, you will receive a response like this:
OK - Deployed application at context path /foo
Otherwise, the response will start with FAIL
and include an
error message. Possible causes for problems include:
- Application already exists at path /foo
The context paths for all currently running web applications must be unique. Therefore, you must undeploy the existing web application using this context path, or choose a different context path for the new one. The
update
parameter may be specified as a parameter on the URL, with a value oftrue
to avoid this error. In that case, an undeploy will be performed on an existing application before performing the deployment. - Document base does not exist or is not a readable directory
The URL specified by the
war
parameter must identify a directory on this server that contains the "unpacked" version of a web application, or the absolute URL of a web application archive (WAR) file that contains this application. Correct the value specified by thewar
parameter. - Encountered exception
An exception was encountered trying to start the new web application. Check the Tomcat logs for the details, but likely explanations include problems parsing your
/WEB-INF/web.xml
file, or missing classes encountered when initializing application event listeners and filters. - Invalid application URL was specified
The URL for the directory or web application that you specified was not valid. Such URLs must start with
file:
, and URLs for a WAR file must end in ".war". - Invalid context path was specified
The context path must start with a slash character. To reference the ROOT web application use "/".
- Context path must match the directory or WAR file name:
If the application war or directory is installed in your Host appBase directory and either the Host is configured with autoDeploy=true the Context path must match the directory name or war file name without the ".war" extension.
- Only web applications in the Host web application directory can
be installed
If the Host deployXML flag is set to false this error will happen if an attempt is made to deploy a web application directory or ".war" file outside of the Host appBase directory.
List Currently Deployed Applications
http://localhost:8080/manager/text/list
List the context paths, current status (running
or
stopped
), and number of active sessions for all currently
deployed web applications. A typical response immediately
after starting Tomcat might look like this:
OK - Listed applications for virtual host localhost
/webdav:running:0:webdav
/examples:running:0:examples
/manager:running:0:manager
/:running:0:ROOT
/test:running:0:test##2
/test:running:0:test##1
Reload An Existing Application
http://localhost:8080/manager/text/reload?path=/examples
Signal an existing application to shut itself down and reload. This can
be useful when the web application context is not reloadable and you have
updated classes or property files in the /WEB-INF/classes
directory or when you have added or updated jar files in the
/WEB-INF/lib
directory.
If this command succeeds, you will see a response like this:
OK - Reloaded application at context path /examples
Otherwise, the response will start with FAIL
and include an
error message. Possible causes for problems include:
- Encountered exception
An exception was encountered trying to restart the web application. Check the Tomcat logs for the details.
- Invalid context path was specified
The context path must start with a slash character. To reference the ROOT web application use "/".
- No context exists for path /foo
There is no deployed application on the context path that you specified.
- No context path was specified
The
path
parameter is required. - Reload not supported on WAR deployed at path /foo
Currently, application reloading (to pick up changes to the classes or
web.xml
file) is not supported when a web application is deployed directly from a WAR file. It only works when the web application is deployed from an unpacked directory. If you are using a WAR file, you shouldundeploy
and thendeploy
ordeploy
with theupdate
parameter the application again to pick up your changes.
List OS and JVM Properties
http://localhost:8080/manager/text/serverinfo
Lists information about the Tomcat version, OS, and JVM properties.
If an error occurs, the response will start with FAIL
and
include an error message. Possible causes for problems include:
- Encountered exception
An exception was encountered trying to enumerate the system properties. Check the Tomcat logs for the details.
List Available Global JNDI Resources
http://localhost:8080/manager/text/resources[?type=xxxxx]
List the global JNDI resources that are available for use in resource
links for context configuration files. If you specify the type
request parameter, the value must be the fully qualified Java class name of
the resource type you are interested in (for example, you would specify
javax.sql.DataSource
to acquire the names of all available
JDBC data sources). If you do not specify the type
request
parameter, resources of all types will be returned.
Depending on whether the type
request parameter is specified
or not, the first line of a normal response will be:
OK - Listed global resources of all types
or
OK - Listed global resources of type xxxxx
followed by one line for each resource. Each line is composed of fields delimited by colon characters (":"), as follows:
- Global Resource Name - The name of this global JNDI resource,
which would be used in the
global
attribute of a<ResourceLink>
element. - Global Resource Type - The fully qualified Java class name of this global JNDI resource.
If an error occurs, the response will start with FAIL
and
include an error message. Possible causes for problems include:
- Encountered exception
An exception was encountered trying to enumerate the global JNDI resources. Check the Tomcat logs for the details.
- No global JNDI resources are available
The Tomcat server you are running has been configured without global JNDI resources.
Session Statistics
http://localhost:8080/manager/text/sessions?path=/examples
Display the default session timeout for a web application, and the
number of currently active sessions that fall within one-minute ranges of
their actual timeout times. For example, after restarting Tomcat and then
executing one of the JSP samples in the /examples
web app,
you might get something like this:
OK - Session information for application at context path /examples
Default maximum session inactive interval 30 minutes
<1 minutes: 1 sessions
1 - <2 minutes: 1 sessions
Expire Sessions
http://localhost:8080/manager/text/expire?path=/examples&idle=num
Display the session statistics (like the above /sessions
command) and expire sessions that are idle for longer than num
minutes. To expire all sessions, use &idle=0
.
OK - Session information for application at context path /examples
Default maximum session inactive interval 30 minutes
1 - <2 minutes: 1 sessions
3 - <4 minutes: 1 sessions
>0 minutes: 2 sessions were expired
Actually /sessions
and /expire
are synonyms for
the same command. The difference is in the presence of idle
parameter.
Start an Existing Application
http://localhost:8080/manager/text/start?path=/examples
Signal a stopped application to restart, and make itself available again. Stopping and starting is useful, for example, if the database required by your application becomes temporarily unavailable. It is usually better to stop the web application that relies on this database rather than letting users continuously encounter database exceptions.
If this command succeeds, you will see a response like this:
OK - Started application at context path /examples
Otherwise, the response will start with FAIL
and include an
error message. Possible causes for problems include:
- Encountered exception
An exception was encountered trying to start the web application. Check the Tomcat logs for the details.
- Invalid context path was specified
The context path must start with a slash character. To reference the ROOT web application use "/".
- No context exists for path /foo
There is no deployed application on the context path that you specified.
- No context path was specified
The
path
parameter is required.
Stop an Existing Application
http://localhost:8080/manager/text/stop?path=/examples
Signal an existing application to make itself unavailable, but leave it deployed. Any request that comes in while an application is stopped will see an HTTP error 404, and this application will show as "stopped" on a list applications command.
If this command succeeds, you will see a response like this:
OK - Stopped application at context path /examples
Otherwise, the response will start with FAIL
and include an
error message. Possible causes for problems include:
- Encountered exception
An exception was encountered trying to stop the web application. Check the Tomcat logs for the details.
- Invalid context path was specified
The context path must start with a slash character. To reference the ROOT web application use "/".
- No context exists for path /foo
There is no deployed application on the context path that you specified.
- No context path was specified
The
path
parameter is required.
Undeploy an Existing Application
http://localhost:8080/manager/text/undeploy?path=/examples
WARNING - This command will delete any web
application artifacts that exist within appBase
directory
(typically "webapps") for this virtual host.
This will delete the application .WAR, if present,
the application directory resulting either from a deploy in unpacked form
or from .WAR expansion as well as the XML Context definition from
$CATALINA_BASE/conf/[enginename]/[hostname]/
directory.
If you simply want to take an application
out of service, you should use the /stop
command instead.
Signal an existing application to gracefully shut itself down, and
remove it from Tomcat (which also makes this context path available for
reuse later). In addition, the document root directory is removed, if it
exists in the appBase
directory (typically "webapps") for
this virtual host. This command is the logical opposite of the
/deploy
command.
If this command succeeds, you will see a response like this:
OK - Undeployed application at context path /examples
Otherwise, the response will start with FAIL
and include an
error message. Possible causes for problems include:
- Encountered exception
An exception was encountered trying to undeploy the web application. Check the Tomcat logs for the details.
- Invalid context path was specified
The context path must start with a slash character. To reference the ROOT web application use "/".
- No context exists named /foo
There is no deployed application with the name that you specified.
- No context path was specified
The
path
parameter is required.
Finding memory leaks
http://localhost:8080/manager/text/findleaks[?statusLine=[true|false]]
The find leaks diagnostic triggers a full garbage collection. It should be used with extreme caution on production systems.
The find leaks diagnostic attempts to identify web applications that have caused memory leaks when they were stopped, reloaded or undeployed. Results should always be confirmed with a profiler. The diagnostic uses additional functionality provided by the StandardHost implementation. It will not work if a custom host is used that does not extend StandardHost.
Explicitly triggering a full garbage collection from Java code is documented
to be unreliable. Furthermore, depending on the JVM used, there are options to
disable explicit GC triggering, like -XX:+DisableExplicitGC
.
If you want to make sure, that the diagnostics were successfully running a full
GC, you will need to check using tools like GC logging, JConsole or similar.
If this command succeeds, you will see a response like this:
/leaking-webapp
If you wish to see a status line included in the response then include the
statusLine
query parameter in the request with a value of
true
.
Each context path for a web application that was stopped, reloaded or undeployed, but which classes from the previous runs are still loaded in memory, thus causing a memory leak, will be listed on a new line. If an application has been reloaded several times, it may be listed several times.
If the command does not succeed, the response will start with
FAIL
and include an error message.
Connector SSL/TLS cipher information
http://localhost:8080/manager/text/sslConnectorCiphers
The SSL Connector/Ciphers diagnostic lists the SSL/TLS ciphers that are currently configured for each connector. For NIO and NIO2, the names of the individual cipher suites are listed. For APR, the value of SSLCipherSuite is returned.
The response will look something like this:
OK - Connector / SSL Cipher information
Connector[HTTP/1.1-8080]
SSL is not enabled for this connector
Connector[HTTP/1.1-8443]
TLS_ECDH_RSA_WITH_3DES_EDE_CBC_SHA
TLS_DHE_RSA_WITH_AES_128_CBC_SHA
TLS_ECDH_RSA_WITH_AES_128_CBC_SHA
TLS_ECDH_ECDSA_WITH_AES_128_CBC_SHA
...
Connector SSL/TLS certificate chain information
http://localhost:8080/manager/text/sslConnectorCerts
The SSL Connector/Certs diagnostic lists the certificate chain that is currently configured for each virtual host.
The response will look something like this:
OK - Connector / Certificate Chain information
Connector[HTTP/1.1-8080]
SSL is not enabled for this connector
Connector[HTTP/1.1-8443]-_default_-RSA
[
[
Version: V3
Subject: CN=localhost, OU=Apache Tomcat PMC, O=The Apache Software Foundation, L=Wakefield, ST=MA, C=US
Signature Algorithm: SHA256withRSA, OID = 1.2.840.113549.1.1.11
...
Connector SSL/TLS trusted certificate information
http://localhost:8080/manager/text/sslConnectorTrustedCerts
The SSL Connector/Certs diagnostic lists the trusted certificates that are currently configured for each virtual host.
The response will look something like this:
OK - Connector / Trusted Certificate information
Connector[HTTP/1.1-8080]
SSL is not enabled for this connector
Connector[AJP/1.3-8009]
SSL is not enabled for this connector
Connector[HTTP/1.1-8443]-_default_
[
[
Version: V3
Subject: CN=Apache Tomcat Test CA, OU=Apache Tomcat PMC, O=The Apache Software Foundation, L=Wakefield, ST=MA, C=US
...
Reload TLS configuration
http://localhost:8080/manager/text/sslReload?tlsHostName=name
Reload the TLS configuration files (the certificate and key files, this does
not trigger a re-parsing of server.xml). To reload the files for all hosts don't
specify the tlsHostName
parameter.
OK - Reloaded TLS configuration for [_default_]
Thread Dump
http://localhost:8080/manager/text/threaddump
Write a JVM thread dump.
The response will look something like this:
OK - JVM thread dump
2014-12-08 07:24:40.080
Full thread dump Java HotSpot(TM) Client VM (25.25-b02 mixed mode):
"http-nio-8080-exec-2" Id=26 cpu=46800300 ns usr=46800300 ns blocked 0 for -1 ms waited 0 for -1 ms
java.lang.Thread.State: RUNNABLE
locks java.util.concurrent.ThreadPoolExecutor$Worker@1738ad4
at sun.management.ThreadImpl.dumpThreads0(Native Method)
at sun.management.ThreadImpl.dumpAllThreads(ThreadImpl.java:446)
at org.apache.tomcat.util.Diagnostics.getThreadDump(Diagnostics.java:440)
at org.apache.tomcat.util.Diagnostics.getThreadDump(Diagnostics.java:409)
at org.apache.catalina.manager.ManagerServlet.threadDump(ManagerServlet.java:557)
at org.apache.catalina.manager.ManagerServlet.doGet(ManagerServlet.java:371)
at javax.servlet.http.HttpServlet.service(HttpServlet.java:618)
at javax.servlet.http.HttpServlet.service(HttpServlet.java:725)
...
VM Info
http://localhost:8080/manager/text/vminfo
Write some diagnostic information about Java Virtual Machine.
The response will look something like this:
OK - VM info
2014-12-08 07:27:32.578
Runtime information:
vmName: Java HotSpot(TM) Client VM
vmVersion: 25.25-b02
vmVendor: Oracle Corporation
specName: Java Virtual Machine Specification
specVersion: 1.8
specVendor: Oracle Corporation
managementSpecVersion: 1.2
name: ...
startTime: 1418012458849
uptime: 393855
isBootClassPathSupported: true
OS information:
...
Save Configuration
http://localhost:8080/manager/text/save
If specified without any parameters, this command saves the current configuration of the server to server.xml. The existing file will be renamed as a backup if required.
If specified with a path
parameter that matches the path of
a deployed web application then the configuration for that web application will
be saved to an appropriately named context.xml file in the xmlBase
for the current Host.
To use the command a StoreConfig MBean must be present. Typically this is configured using the StoreConfigLifecycleListener.
If the command does not succeed, the response will start with
FAIL
and include an error message.
Server Status
From the following links you can view Status information about the server. Any one of manager-xxx roles allows access to this page.
http://localhost:8080/manager/status
http://localhost:8080/manager/status/all
Displays server status information in HTML format.
http://localhost:8080/manager/status?XML=true
http://localhost:8080/manager/status/all?XML=true
Displays server status information in XML format.
First, you have the server and JVM version number, JVM provider, OS name and number followed by the architecture type.
Second, there is information about the memory usage of the JVM.
Then, there is information about the Tomcat AJP and HTTP connectors. The same information is available for both of them :
Threads information : Max threads, min and max spare threads, current thread count and current thread busy.
Request information : Max processing time and processing time, request and error count, bytes received and sent.
A table showing Stage, Time, Bytes Sent, Bytes Receive, Client, VHost and Request. All existing threads are listed in the table. Here is the list of the possible thread stages :
"Parse and Prepare Request" : The request headers are being parsed or the necessary preparation to read the request body (if a transfer encoding has been specified) is taking place.
"Service" : The thread is processing a request and generating the response. This stage follows the "Parse and Prepare Request" stage and precedes the "Finishing" stage. There is always at least one thread in this stage (the server-status page).
"Finishing" : The end of the request processing. Any remainder of the response still in the output buffers is sent to the client. This stage is followed by "Keep-Alive" if it is appropriate to keep the connection alive or "Ready" if "Keep-Alive" is not appropriate.
"Keep-Alive" : The thread keeps the connection open to the client in case the client sends another request. If another request is received, the next stage will be "Parse and Prepare Request". If no request is received before the keep alive times out, the connection will be closed and the next stage will be "Ready".
"Ready" : The thread is at rest and ready to be used.
If you are using /status/all
command, additional information
on each of deployed web applications will be available.
Using the JMX Proxy Servlet
What is JMX Proxy Servlet
JMX Query command
This takes the form:
http://webserver/manager/jmxproxy/?qry=STUFF
Where STUFF
is the JMX query you wish to perform. For example,
here are some queries you might wish to run:
-
qry=*%3Atype%3DRequestProcessor%2C* --> type=RequestProcessor
which will locate all workers which can process requests and report their state. -
qry=*%3Aj2eeType=Servlet%2c* --> j2eeType=Servlet
which return all loaded servlets. -
qry=Catalina%3Atype%3DEnvironment%2Cresourcetype%3DGlobal%2Cname%3DsimpleValue --> Catalina:type=Environment,resourcetype=Global,name=simpleValue
which look for a specific MBean by the given name.
You'll need to experiment with this to really understand its capabilities
If you provide no qry
parameter, then all of the MBeans will
be displayed. We really recommend looking at the tomcat source code and
understand the JMX spec to get a better understanding of all the queries
you may run.
JMX Get command
The JXMProxyServlet also supports a "get" command that you can use to
fetch the value of a specific MBean's attribute. The general form of
the get
command is:
http://webserver/manager/jmxproxy/?get=BEANNAME&att=MYATTRIBUTE&key=MYKEY
You must provide the following parameters:
get
: The full bean nameatt
: The attribute you wish to fetchkey
: (optional) The key into a CompositeData MBean attribute
If all goes well, then it will say OK, otherwise an error message will be shown. For example, let's say we wish to fetch the current heap memory data:
http://webserver/manager/jmxproxy/?get=java.lang:type=Memory&att=HeapMemoryUsage
Or, if you only want the "used" key:
http://webserver/manager/jmxproxy/
?get=java.lang:type=Memory&att=HeapMemoryUsage&key=used
JMX Set command
Now that you can query an MBean, its time to muck with Tomcat's internals! The general form of the set command is :
http://webserver/manager/jmxproxy/?set=BEANNAME&att=MYATTRIBUTE&val=NEWVALUE
So you need to provide 3 request parameters:
set
: The full bean nameatt
: The attribute you wish to alterval
: The new value
If all goes ok, then it will say OK, otherwise an error message will be
shown. For example, lets say we wish to turn up debugging on the fly for the
ErrorReportValve
. The following will set debugging to 10.
http://localhost:8080/manager/jmxproxy/
?set=Catalina%3Atype%3DValve%2Cname%3DErrorReportValve%2Chost%3Dlocalhost
&att=debug&val=10
and my result is (YMMV):
Result: ok
Here is what I see if I pass in a bad value. Here is the URL I used, I try set debugging equal to 'cow':
http://localhost:8080/manager/jmxproxy/
?set=Catalina%3Atype%3DValve%2Cname%3DErrorReportValve%2Chost%3Dlocalhost
&att=debug&val=cow
When I try that, my result is
Error: java.lang.NumberFormatException: For input string: "cow"
JMX Invoke command
The invoke
command enables methods to be called on MBeans. The
general form of the command is:
http://webserver/manager/jmxproxy/
?invoke=BEANNAME&op=METHODNAME&ps=COMMASEPARATEDPARAMETERS
For example, to call the findConnectors()
method of the
Service use:
http://localhost:8080/manager/jmxproxy/
?invoke=Catalina%3Atype%3DService&op=findConnectors&ps=
Executing Manager Commands With Ant
In addition to the ability to execute Manager commands via HTTP requests, as documented above, Tomcat includes a convenient set of Task definitions for the Ant (version 1.4 or later) build tool. In order to use these commands, you must perform the following setup operations:
- Download the binary distribution of Ant from http://ant.apache.org. You must use version 1.4 or later.
- Install the Ant distribution in a convenient directory (called ANT_HOME in the remainder of these instructions).
- Add the
$ANT_HOME/bin
directory to yourPATH
environment variable. - Configure at least one username/password combination in your Tomcat
user database that includes the
manager-script
role.
To use custom tasks within Ant, you must declare them first with an
<import>
element. Therefore, your build.xml
file might look something like this:
<project name="My Application" default="compile" basedir=".">
<!-- Configure the directory into which the web application is built -->
<property name="build" value="${basedir}/build"/>
<!-- Configure the context path for this application -->
<property name="path" value="/myapp"/>
<!-- Configure properties to access the Manager application -->
<property name="url" value="http://localhost:8080/manager/text"/>
<property name="username" value="myusername"/>
<property name="password" value="mypassword"/>
<!-- Configure the path to the Tomcat installation -->
<property name="catalina.home" value="/usr/local/apache-tomcat"/>
<!-- Configure the custom Ant tasks for the Manager application -->
<import file="${catalina.home}/bin/catalina-tasks.xml"/>
<!-- Executable Targets -->
<target name="compile" description="Compile web application">
<!-- ... construct web application in ${build} subdirectory, and
generated a ${path}.war ... -->
</target>
<target name="deploy" description="Install web application"
depends="compile">
<deploy url="${url}" username="${username}" password="${password}"
path="${path}" war="file:${build}${path}.war"/>
</target>
<target name="reload" description="Reload web application"
depends="compile">
<reload url="${url}" username="${username}" password="${password}"
path="${path}"/>
</target>
<target name="undeploy" description="Remove web application">
<undeploy url="${url}" username="${username}" password="${password}"
path="${path}"/>
</target>
</project>
Note: The definition of the resources task via the import above will override
the resources datatype added in Ant 1.7. If you wish to use the resources
datatype you will need to use Ant's namespace support to modify
catalina-tasks.xml
to assign the Tomcat tasks to their own
namespace.
Now, you can execute commands like ant deploy
to deploy the
application to a running instance of Tomcat, or ant reload
to
tell Tomcat to reload it. Note also that most of the interesting values in
this build.xml
file are defined as replaceable properties, so
you can override their values from the command line. For example, you might
consider it a security risk to include the real manager password in your
build.xml
file's source code. To avoid this, omit the password
property, and specify it from the command line:
ant -Dpassword=secret deploy
Tasks output capture
Using Ant version 1.6.2 or later,
the Catalina tasks offer the option to capture their output in
properties or external files. They support directly the following subset of the
<redirector>
type attributes:
Attribute | Description | Required |
---|---|---|
output | Name of a file to which to write the output. If the error stream is not also redirected to a file or property, it will appear in this output. | No |
error | The file to which the standard error of the command should be redirected. | No |
logError | This attribute is used when you wish to see error output in Ant's log and you are redirecting output to a file/property. The error output will not be included in the output file/property. If you redirect error with the error or errorProperty attributes, this will have no effect. | No |
append | Whether output and error files should be
appended to or overwritten. Defaults to false . |
No |
createemptyfiles | Whether output and error files should be created
even when empty. Defaults to true . |
No |
outputproperty | The name of a property in which the output of the command should be stored. Unless the error stream is redirected to a separate file or stream, this property will include the error output. | No |
errorproperty | The name of a property in which the standard error of the command should be stored. | No |
A couple of additional attributes can also be specified:
Attribute | Description | Required |
---|---|---|
alwaysLog | This attribute is used when you wish to see the
output you are capturing, appearing also in the Ant's log. It must not be
used unless you are capturing task output.
Defaults to false .
This attribute will be supported directly by <redirector>
in Ant 1.6.3 |
No |
failonerror | This attribute is used when you wish to avoid that
any manager command processing error terminates the ant execution. Defaults to true .
It must be set to false , if you want to capture error output,
otherwise execution will terminate before anything can be captured.
This attribute acts only on manager command execution, any wrong or missing command attribute will still cause Ant execution termination. |
No |
They also support the embedded <redirector>
element
in which you can specify
its full set of attributes, but input
, inputstring
and
inputencoding
that, even if accepted, are not used because they have
no meaning in this context.
Refer to ant manual for details on
<redirector>
element attributes.
Here is a sample build file extract that shows how this output redirection support can be used:
<target name="manager.deploy"
depends="context.status"
if="context.notInstalled">
<deploy url="${mgr.url}"
username="${mgr.username}"
password="${mgr.password}"
path="${mgr.context.path}"
config="${mgr.context.descriptor}"/>
</target>
<target name="manager.deploy.war"
depends="context.status"
if="context.deployable">
<deploy url="${mgr.url}"
username="${mgr.username}"
password="${mgr.password}"
update="${mgr.update}"
path="${mgr.context.path}"
war="${mgr.war.file}"/>
</target>
<target name="context.status">
<property name="running" value="${mgr.context.path}:running"/>
<property name="stopped" value="${mgr.context.path}:stopped"/>
<list url="${mgr.url}"
outputproperty="ctx.status"
username="${mgr.username}"
password="${mgr.password}">
</list>
<condition property="context.running">
<contains string="${ctx.status}" substring="${running}"/>
</condition>
<condition property="context.stopped">
<contains string="${ctx.status}" substring="${stopped}"/>
</condition>
<condition property="context.notInstalled">
<and>
<isfalse value="${context.running}"/>
<isfalse value="${context.stopped}"/>
</and>
</condition>
<condition property="context.deployable">
<or>
<istrue value="${context.notInstalled}"/>
<and>
<istrue value="${context.running}"/>
<istrue value="${mgr.update}"/>
</and>
<and>
<istrue value="${context.stopped}"/>
<istrue value="${mgr.update}"/>
</and>
</or>
</condition>
<condition property="context.undeployable">
<or>
<istrue value="${context.running}"/>
<istrue value="${context.stopped}"/>
</or>
</condition>
</target>
WARNING: even if it doesn't make many sense, and is always a bad idea, calling a Catalina task more than once, badly set Ant tasks depends chains may cause that a task be called more than once in the same Ant run, even if not intended to. A bit of caution should be exercised when you are capturing output from that task, because this could lead to something unexpected:
- when capturing in a property you will find in it only the output from the first call, because Ant properties are immutable and once set they cannot be changed,
- when capturing in a file, each run will overwrite it and you will find in it only the last call
output, unless you are using the
append="true"
attribute, in which case you will see the output of each task call appended to the file.